顧客への持続可能性の影響
サステナビリティに対する情熱とコミットメントを持つ、シュナイダーエレクトリックのパートナーである場合は、このノミネーションを受理します。アワードは、チームとビジネスに大きな変革をもたらす可能性があります。今すぐ会社をノミネーションしてください。
Participate multiple times!
個人のチャレンジ
LJ Services
Delivered a data ready building management solution through system design and install. Our work underpins a solution that will help our client achieve their sustainability targets, continuously improve their environmental impact and deliver ESG reporting
ドキュメント
LJ Services
簡単な会社説明
Delivered a data ready building management solution through system design and install. Our work underpins a solution that will help our client achieve their sustainability targets, continuously improve their environmental impact and deliver ESG reporting
位置
Australia
私は:
システムインテグレータ
セグメントタイプ:
商業不動産
会社規模
0~5千万ユーロ
これらの結果に対する最高責任者がいますか? その場合は、名前とメールアドレスをお知らせください。
Leigh Booth; leigh@ljservices.com.au
私はシュナイダーエレクトリックの担当者のサポートを受けています。 はい」の場合、シュナイダーエレクトリックの担当者名をご記入ください。
Gus Alveraz
1. 戦略立案をおこなっていますか?
いいえ
A.顧客には、マイルストーンを伴う脱炭素化プランがありますか? その場合は、ロードマップ/プランを共有してください。
未返信B.お客様またはその顧客はシュナイダーエレクトリックのサステナビリティスクールのすべてのクラスを修了していますか?
未返信2. デジタル化していますか?
はい
A.顧客のエネルギーと二酸化炭素の分析およびレポート用の一元的なユーティリティデータの管理および監視ソフトウェアの導入を支援していますか?
We worked with our client to develop and install a strategic solution across their building portfolio that delivers accurate and timely data across key meter points. This data will be extracted into a data management and monitoring solution and will help our client to make informed decisions with respect to their energy consumption, production and carbon emissions. Previously, energy data was missing and ad hoc which affected both reporting accuracy and optimal load management, potentially adding to higher than necessary energy consumption and emissions. We designed and installed a system to address this and make our client’s building portfolio data ready, providing accurate and timely data across multiple devices which can be accessed by anyone. This data has enabled the client to be able to collate information easily and often through extraction into their reporting systems, in order for them to take corrective actions that will improve the efficiency and effectiveness of their energy solutions. The outcome of the building data provided will help our client to achieve their sustainability targets, improve their sustainability rating (as measured by NABERS) and support them to deliver their ESG reporting requirements.
B.お客様の支援によって、顧客はエネルギー消費量と排出量を削減する機会を見つけるために、主要なエネルギー負荷を計測していますか?
Yes, we worked collaboratively with our client to replace current systems and install capability that meters their major energy loads across a portfolio of 5 commercial buildings. With this data, the client is able to make informed decisions at an aggregate level to optimise load and take advantage of opportunities to reduce energy consumption. This will help our client make strategic decisions to achieve their sustainability targets and reduce their carbon footprint.
C.顧客がエネルギー効率と機器のパフォーマンスを監視し、実践的な洞察を得られるよう支援していますか?
Yes, we are providing the data and the insights into a data management system and we are using that system to help the client drive efficiencies across their portfolio. We have designed the building automation and building services to ensure that all the information is ready for anyone to capture, aggregate and develop actionable insights. We are working with the client to help them with the performance of their equipment.
D.顧客は、電力管理およびモニタリングソリューションを使用して、パワーの質を評価し、ビジネスの回復力と継続性を向上させることができるでしょうか。
E.顧客を代表して、業務の効率とデジタル化を最大化するイノベーションを導入しましたか?
Yes, we have implemented optimisation on various building services (e.g. electrical and hydraulic metering and general HVAC services). This will help our client to optimise their energy usage across their building portfolio and to also help their clients who are tenants of the building, to optimise their energy consumption and running costs. This supports our client to both save money and gain access to better clients as they are all seeking access to 5 star rated buildings.
F.顧客がプラント機器の寿命を最適化して延ばし、排出ガスを回避できるように、資産のアップグレードと近代化プログラムを導入していますか?
No, not yet but this is in planning and the system deployed will support this activity . Of particular interest are replacement of legacy Gas Fired systems with Electric Heat pumps
G.顧客のプロセスを最適化しながらパワー消費量を最小限に抑える方法として、エネルギーとプロセスのデジタル統合を取り入れましたか?
Our team are our client’s champions , we encourage new technology in every instance.
3. 脱炭素化をしていますか?
はい
A.顧客は自動化およびエネルギー管理システムを使用して、機器とシステムを制御できるようになっていますか?
We are
B.顧客は、ご支援の下、エネルギー効率を向上させるプラクティスを導入していますか?
未返信C.顧客が、エネルギー需要の少なくとも一部に再生可能エネルギー(PPA、EAC、またはオンサイト発電)を使用できるようにしていますか?
Nil at this stage
D.スコープ2排出量を最小化するために、顧客がオフサイトの再生可能エネルギーパワー購入契約またはエネルギー属性証明書を通じてエネルギーを調達するのを支援しましたか。
未返信E.顧客は、顧客の助けを借りて、オンサイトの再生可能エネルギー発電の電力を使用してスコープ2排出を削減していますか?
F.顧客のためにエネルギー貯蔵を導入していますか?
未返信G.顧客に分散型発電資産を集約して、経済的価値とグリッドへの影響を最大化させる態勢を整えていますか?
未返信H.顧客の業務におけるエネルギー効率と脱炭素に重点を置くことで、二酸化炭素排出量を削減していますか?
I.顧客は、エネルギー効率と脱炭素に重点を置いた最新化プロジェクトを通じて二酸化炭素排出量を削減していますか?
No, not yet but this is in planning and the system deployed will support this activity . Of particular interest are replacement of legacy Gas Fired systems with Electric Heat pumps
J.顧客の業務において、エネルギー効率を高める慣行を実施するお手伝いをしたことがありますか?
未返信K.顧客がサプライヤーとスコープ3排出量を削減するコミットメントプログラムを作成するのを支援しましたか?
未返信L.顧客は、顧客の支援の下、上流のサプライヤーおよび下流の流通パートナーとスコープ3排出量の追跡と削減に関するコミットメントプログラムを採用しましたか?
未返信M.顧客がデジタルモデリングを使用して、材料や機器から具現化されたカーボンデータをキャプチャできるようにしましたか?
N.顧客が、船舶、従業員、顧客のために電気自動車の充電インフラを運用に組み込むのを支援してきましたか?
As the EV charging Badge is very new to our offer arsenal, we are currently reviewing existing portfolio sites for suitability.
O.顧客のご案内によって、車両の一部を電気自動車に改造したことがありますか?
P.顧客が、スコープ1排出を削減するために事業の一部に通電できるようにして、再生可能エネルギーを使用して二酸化炭素排出量を削減できるようにしましたか? 顧客の業務のうち、どの程度の割合が電化されていますか?
未返信Q.低炭素の材料や設備を購入するよう顧客にアドバイスしましたか。
We offer Low Smoke Zero Halogen ( LSZH) cabling as an option to projects for consideration should cost restraints not inhibit.
R.顧客はコンディションベースのメンテナンスを活用して、機器の寿命を延ばし、新しい機器の購入を遅らせ、関連する具体的なカーボンを削減していますか?
This will be the outcome of currently installed BMS solution once historical data is proven and reviewed.
S.顧客のアドバイスに基づいて、顧客はスコープ1とスコープ3の残留排出量のバランスを取るためにカーボンオフセットを購入していますか?
未返信T.顧客が運用を改善して効率を重視できるようにして、水の使用量を削減できるようにお手伝いしていますか?
未返信U.顧客が、水の可用性に関するリスクと予測に基づいて水の使用量を監視し、調整できるようにしましたか?
We monitor potable and Non-Potable ( Rainwater) for usage and management.
V.顧客が、効率を重視する浄水と廃水の処理および回収プログラムなど、クリーンインプレイスオペレーションの最適化プログラムを作成するお手伝いをしたことがありますか?
未返信W.顧客は循環型資材を調達し、業務の無駄を最小限に抑えていますか?
未返信X.顧客の化石エネルギーベースのプロセスを電化に移行する計画の策定を支援しましたか?
No, not yet but this is in planning and the system deployed will support this activity . Of particular interest are replacement of legacy Gas Fired systems with Electric Heat pumps
Y(i)。顧客の技術革新や循環型ビジネスモデルの展開を支援してきましたか? 当てはまるものすべてをお選びください。
- 顧客の業務におけるエネルギー消費と二酸化炭素排出量を削減するイノベーションの導入を支援しましたか?
- 顧客がエネルギー源を再生可能エネルギーに置き換えるイノベーションを展開する支援をしましたか?
- 顧客の水使用量を減らすイノベーションの展開をサポートしましたか?
Y(ii). こうした技術革新の成果について教えてください。
The results are still pending
追加ドキュメント(存在する場合)
未返信Translation (when applicable)
未返信
コメント