可持续影响力合作伙伴奖
如果您是一位对可持续发展充满热情并为此做出承诺的施耐德电气合作伙伴,我们希望收到您的报名申请。该奖项对于您的团队和企业而言都是一项真正的变革 — 快来提名您的公司吧!
Participate multiple times!
个人
挑战
GSTEC
A complete replacement of existing Siemens Building Management System with Schneider Electric EcoStruxure Building Operation platform, incorporating a Building Management and Energy management System, BACnet IP SmartX controllers and Space Logic sensors.
文档
Participation form
GSTEC
公司简介
A complete replacement of existing Siemens Building Management System with Schneider Electric EcoStruxure Building Operation platform, incorporating a Building Management and Energy management System, BACnet IP SmartX controllers and Space Logic sensors.
地点
Australia
我是:
系统集成商
细分类型
商业房地产
公司规模
0 - 5,000 万欧元
贵公司中是否有人对这些结果的责任人? 如果有,请提供其姓名和电子邮件地址。
Doug McMillan, dmc@gstec.com.au; Ian Sweeting isw@gstc.com.au
我已获得施耐德电气联系人的支持。 如果 "是",请注明您的施耐德电气联系人姓名。
Monica Keith
1. 您是否有制定了可持续发展战略?
是
A. 您是否制定了一个具有里程碑意义的减碳计划? 如果是,请分享您的计划或实行路径。
未回复B. 您或您的客户是否完成施耐德电气可持续发展学校的所有课程?
未回复2. 您是否有实行数字化?
是
A. 您是否帮助客户部署了集中式公用事业数据管理和监控软件,用于能源和碳分析及报告?
As part of our digitisation of the buildings electrical infrastructure the project included the establishment of digital connectivity with key components of the electrical distribution system including, air circuit breakers and circuit protection devices in the main switchboards; backup generator control and fuel transfer system PLCs; automatic transfer switches; uninterruptable power supplies; and variable frequency drives. The building operator has committed to the future deployment of electric vehicle (EV) chargers in the buildings carpark and planning is underway to integrate the chargers with the electrical infrastructure using EBO.
B. 在您的帮助下,客户是否会计量主要能源负载,以发现降低能耗和排放的机会?
The decarbonisation strategy for Aurora Place primarily involves firstly, the digitisation and integration of building components including the HVAC system, the electrical infrastructure, access control system and other building services through the new integrated communications network (ICN). Secondly, the utilisation of the new energy management system (EMS) to identify excess energy usage and optimisation opportunities. Thirdly, to use the capabilities of the EcoStruxure Building Operation (EBO) platform including its ability to incorporate and act on external data (e.g. weather data) to realise and maintain optimal building energy consumption.
C. 您是否进行能源效率的监控?根据设备性能和数据表现,是否有一些见解可以分享?
GSTEC are currently in discussions with the building operators regarding the use of Schneider EcoStruxure Building Advisor or other cloud based analytics product to provide monitoring and insights into building operations to support the sustainability objectives.
D. 您是否支持客户使用电源管理和监控解决方案来评估电源质量并提高业务弹性和连续性?
GSTEC are currently in discussions with the building operators regarding the use of Schneider EcoStruxure Building Advisor or other cloud based analytics product to provide monitoring and insights into building operations to support the sustainability objectives.
E. 您是否代表客户部署了创新解决方案,以最大程度提高其运营效率并实现运营数字化?
Yes as per the above.
F. 您是否为客户实施了资产升级和现代化升级,以优化和延长工厂设备的使用寿命并避免排放?
G. 您是否为客户实行了电源和流程的数字集成,将其作为最大程度减少能耗并优化流程的一种方法?
未回复3. 您是否采取了减碳措施?
是
A. 您是否正在支持客户使用自动化和能源管理系统来控制其设备和系统?
未回复B. 在您的帮助下,客户是否实施了提高能效的措施?
未回复C. 您是否支持客户使用可再生能源(PPA、EAC 或现场发电)至少满足其一部分能源需求?
未回复D. 您是否通过场外可再生能源购买协议或能源属性证书来获取能源,以最大程度减少范围 2 排放?
未回复E. 在您的帮助下,客户是否正在使用现场可再生能源发电来减少范围 2 排放?
Yes
F. 您是否为客户实施了储能?
G. 您是否为客户提供装备,整合了分散的发电资产,以实现经济价值和电网影响最大化?
No
H. 您是否通过在运营中专注于改善能效来帮助客户减少碳排放?
yes as stated previously above
I. 在您的帮助下,客户是否通过专注于改善能效和减碳的现代化项目减少了碳足迹?
yes as stated previously above
J. 您是否帮助客户实施了提高运营能效的措施?
To achieve our sustainability goals during the project, we planned and managed our activities on site using best practice environmental management principals such as: • Building facilities team provided an allocated storage area within the building for the temporary storage of recycling material • All paper and cardboard packaging was returned to GSTEC warehouse for disposal via GSTEC offsite cardboard recycling process • Packing material and fill was returned to the GSTEC warehouse for reuse by the store person • All metal building waste including mild steel, aluminium, variable speed drives, enclosures, cable trays, and ducting were returned to GSTEC warehouse for transport to Sims Metal recycling facility • All redundant or obsolete electronic devices including network controllers, field controllers, electronic field devices were returned to ToxFree for e-waste recycling and certificates will be included in the project O&M manual • All redundant or obsolete copper and aluminium wiring including power cabling, network cables, control cabling, MIMs cable, was returned to GSTEC warehouse for insulation removal and copper and aluminium recycling • To aid in the reducing the use of paper in this project: o O&M manuals will be provided in soft copy and stored on the BMS server o Installation and design documentation including drawings, network diagrams, functional descriptions etc were provided to field staff in soft copy o It was agreed that consultant mark-ups on soft copy were an acceptable form of approval • Consideration was given to unnecessary energy use during the project, including: o The commissioning equipment during normal operational hours where possible o Using isolation to reduce equipment energy loads during commissioning o Ensuring plant and equipment was commissioned and tuned at the earliest opportunity to prevent inefficient operation • Minimising the use of work vehicles on site and encouraging transport to and from site via public transport, included the provision of transport cards to project staff.
K. 您是否与客户的供应商一起帮助客户开展了承诺计划,以减少其范围 3 排放?
Not yet
L. 在您的帮助下,客户是否与上游供应商和下游分销合作伙伴一起采用了承诺计划以跟踪和减少范围 3 排放?
Not yet
M. 您是否支持客户利用数字建模从材料和设备获取了隐含碳相关数据?
Not yet
N. 您是否帮助客户将电动汽车充电基础设施融入到车队、员工和/或客户的运营中?
Yes
O. 在您的指导下,客户是否将其车队部分车辆改造成电动汽车?
Yes - making the site EV-ready.
P. 您是否支持客户对其部分运营进行电气化改造,以减少范围 1 排放,并支持使用可再生能源来减少碳足迹? 客户运营中的电气化占比是多少?
未回复Q. 您建议客户购买低隐含碳材料和设备了吗?
Yes
R. 在您的帮助下,客户是否借助视情况维护来延长设备使用寿命、延迟购买新设备并减少相关的隐含碳排放?
Yes
S. 根据您的建议,客户是否购买碳补偿以平衡任何范围 1 和范围 3 残余排放?
Not yet
T. 您是否正在通过改善日常运营和关注效率来帮助客户减少用水量?
No
U. 您是否支持客户根据水可用性风险和预测来监控和调整用水量?
No
V. 您是否帮助客户创建了现场清洁运营优化计划,如以效率为重点的水和废水处理及回收计划?
No
W. 在您的帮助下,客户是否采购循环材料,并尽量减少产生运营废物?
No
X. 您是否帮助客户制定了将其基于化石能源的流程向电气化流程转型的计划?
No
Y(i). 您是否帮助客户部署了创新技术或循环业务模式? 请选择所有适用项:
帮助客户部署了创新技术以减少其运营的能耗和碳排放?
Y(ii). 这些创新取得了哪些成果?
Please reference above answers.
其他文件(如有)
未回复Translation (when applicable)
未回复
评论