可持续影响力合作伙伴奖
如果您是一位对可持续发展充满热情并为此做出承诺的施耐德电气合作伙伴,我们希望收到您的报名申请。该奖项对于您的团队和企业而言都是一项真正的变革 — 快来提名您的公司吧!
Participate multiple times!
个人
挑战
Civis Villszer Kft.
Our company's main profile is the manufacture, installation and maintenance of high-voltage equipment. We are also a major market player in the installation of charging points for electric vehicles - we installed Hungary's first high power DC charger.
文档
Civis Villszer Kft.
公司简介
Our company's main profile is the manufacture, installation and maintenance of high-voltage equipment. We are also a major market player in the installation of charging points for electric vehicles - we installed Hungary's first high power DC charger.
地点
Hungary
我是:
承包商
细分类型
汽车和弹能
公司规模
0 - 5,000 万欧元
贵公司中是否有人对这些结果的责任人? 如果有,请提供其姓名和电子邮件地址。
Mátyás Csábi csabi.matyas@civisvill.hu
我已获得施耐德电气联系人的支持。 如果 "是",请注明您的施耐德电气联系人姓名。
Tamás Lukács, tamas.lukacs@se.com
1. 您是否有制定了可持续发展战略?
否
A. 您是否制定了一个具有里程碑意义的减碳计划? 如果是,请分享您的计划或实行路径。
未回复B. 您或您的客户是否完成施耐德电气可持续发展学校的所有课程?
未回复2. 您是否有实行数字化?
是
A. 您是否帮助客户部署了集中式公用事业数据管理和监控软件,用于能源和碳分析及报告?
For energy analysis and measurement: Scada. For operation: PMA.
B. 在您的帮助下,客户是否会计量主要能源负载,以发现降低能耗和排放的机会?
It continuously monitors energy use, reports on it, and makes interventions or improvements depending on the results. We do not have accurate data on the analysis of the scale of emissions.
C. 您是否进行能源效率的监控?根据设备性能和数据表现,是否有一些见解可以分享?
With measurement and energy balance monitoring.
D. 您是否支持客户使用电源管理和监控解决方案来评估电源质量并提高业务弹性和连续性?
We offer energy, management and monitoring systems from most major manufacturers, including Schneider Electric, as solutions for our customers (e.g (Aveva Plant Scada, Power Scada). Using monitoring and data collection systems minimise downtime, optimise operation and increase service life.
E. 您是否代表客户部署了创新解决方案,以最大程度提高其运营效率并实现运营数字化?
Yes. The installation of state-of-the-art digital metering and process monitoring systems has contributed greatly to reducing our customers' energy consumption. For example, in the hotel industry, as well as in the service industry, Building Operation software systems have been used to programmatically optimise the uptime of equipment (cooling, heating, lighting), leading to significant cost savings. Significant results have been achieved in terms of increased lifetime (lighting) and reduced energy consumption.
F. 您是否为客户实施了资产升级和现代化升级,以优化和延长工厂设备的使用寿命并避免排放?
For example, using remote monitoring, condition monitoring systems for high-current switchgear, their lifetime can be extended - so that a warranty extension can be achieved. By extending the equipment replacement cycle, we directly contribute to reducing emissions.
G. 您是否为客户实行了电源和流程的数字集成,将其作为最大程度减少能耗并优化流程的一种方法?
Certainly. For our customers, the efficiency and measurable benefits of the first remote metering and monitoring system provided at a discount were so convincing that they subsequently ordered a number of similar installations from our company also for other holdings.
3. 您是否采取了减碳措施?
是
A. 您是否正在支持客户使用自动化和能源管理系统来控制其设备和系统?
We offer almost all relevant systems from many major manufacturers such as Schneider Electric (BMS, PME, Powrer Scada, Aveva plant Scada, EcoStruxure). The efficiencies that can be achieved with these systems are, in our experience, close to the manufacturer's specifications.
B. 在您的帮助下,客户是否实施了提高能效的措施?
C. 您是否支持客户使用可再生能源(PPA、EAC 或现场发电)至少满足其一部分能源需求?
On average, our clients involved in this topic cover at least 10%.
D. 您是否通过场外可再生能源购买协议或能源属性证书来获取能源,以最大程度减少范围 2 排放?
E. 在您的帮助下,客户是否正在使用现场可再生能源发电来减少范围 2 排放?
On average, our customers involved in this topic, produce 10-15% for themselves, occasionally 30%.
F. 您是否为客户实施了储能?
Operational safety increased by reducing the risk of outages, and by breaking down peak energy demands no power overshoots were observed.
G. 您是否为客户提供装备,整合了分散的发电资产,以实现经济价值和电网影响最大化?
H. 您是否通过在运营中专注于改善能效来帮助客户减少碳排放?
I. 在您的帮助下,客户是否通过专注于改善能效和减碳的现代化项目减少了碳足迹?
未回复J. 您是否帮助客户实施了提高运营能效的措施?
未回复K. 您是否与客户的供应商一起帮助客户开展了承诺计划,以减少其范围 3 排放?
未回复L. 在您的帮助下,客户是否与上游供应商和下游分销合作伙伴一起采用了承诺计划以跟踪和减少范围 3 排放?
M. 您是否支持客户利用数字建模从材料和设备获取了隐含碳相关数据?
未回复N. 您是否帮助客户将电动汽车充电基础设施融入到车队、员工和/或客户的运营中?
Our company has installed the first high power (180kW) DC charger (EVD1S180TxB) manufactured by Schneider Electric in the country. This has drastically reduced charging times, resulting in increased vehicle mobility. During the changeover, there was also a noticeable reduction in the cost (Forint) per km for company vehicles when using other types of Evlink chargers. The use of electric vehicles has enabled on-site charging, which also has many benefits for our company (no commuting, no petrol card, we can go tot he location of failure immediately, etc.).
O. 在您的指导下,客户是否将其车队部分车辆改造成电动汽车?
Yes, by installing charging equipment. Approximately 25% of the fleet. 30% of parking spaces can accomodate EVs.
P. 您是否支持客户对其部分运营进行电气化改造,以减少范围 1 排放,并支持使用可再生能源来减少碳足迹? 客户运营中的电气化占比是多少?
Q. 您建议客户购买低隐含碳材料和设备了吗?
We offer products from companies that are committed to manufacturing low-carbon materials and equipment, such as Schneider Electric.
R. 在您的帮助下,客户是否借助视情况维护来延长设备使用寿命、延迟购买新设备并减少相关的隐含碳排放?
Relevant lifetime extensions can be achieved through such maintenance, which involves remote monitoring (Power Scada), visual inspection and multi-stage condition monitoring.
S. 根据您的建议,客户是否购买碳补偿以平衡任何范围 1 和范围 3 残余排放?
T. 您是否正在通过改善日常运营和关注效率来帮助客户减少用水量?
未回复U. 您是否支持客户根据水可用性风险和预测来监控和调整用水量?
未回复V. 您是否帮助客户创建了现场清洁运营优化计划,如以效率为重点的水和废水处理及回收计划?
未回复W. 在您的帮助下,客户是否采购循环材料,并尽量减少产生运营废物?
未回复X. 您是否帮助客户制定了将其基于化石能源的流程向电气化流程转型的计划?
Yes. We can demonstrate the benefits of electrification to our customers by providing them with electric vehicle transition plans.
Y(i). 您是否帮助客户部署了创新技术或循环业务模式? 请选择所有适用项:
- 帮助客户部署了创新技术以减少其运营的能耗和碳排放?
- 帮助客户部署创新解决方案,以最大化其运营电气化?
- 帮助客户部署创新技术以用可再生能源替代传统能源?
- 帮助客户部署创新技术以减少用水量?
Y(ii). 这些创新取得了哪些成果?
In all cases, apparent operating cost savings can be achieved, even in the short term. Factual data on long-term returns are not yet available, as the innovations listed do not yet provide sufficient data to make the appropriate calculations.
其他文件(如有)
未回复Translation (when applicable)
未回复
评论