可持续影响力合作伙伴奖
如果您是一位对可持续发展充满热情并为此做出承诺的施耐德电气合作伙伴,我们希望收到您的报名申请。该奖项对于您的团队和企业而言都是一项真正的变革 — 快来提名您的公司吧!
Participate multiple times!
个人
挑战
PMI Associates
PMI Associates is the oldest SI in India dealing in Power Management Systems, having started it's journey with PML, Canada in 1997 (it got taken over by Schneider in 2005). We have implemented varied solutions to all type of industries across India.
文档
Participation form
PMI Associates
公司简介
PMI Associates is the oldest SI in India dealing in Power Management Systems, having started it's journey with PML, Canada in 1997 (it got taken over by Schneider in 2005). We have implemented varied solutions to all type of industries across India.
地点
India
我是:
系统集成商
细分类型
能源管理
公司规模
0 - 5,000 万欧元
贵公司中是否有人对这些结果的责任人? 如果有,请提供其姓名和电子邮件地址。
Sandeep Sharma sandeep.sharma@pmiassociates.com
我已获得施耐德电气联系人的支持。 如果 "是",请注明您的施耐德电气联系人姓名。
Yes, Hariom Jha
1. 您是否有制定了可持续发展战略?
否
A. 您是否制定了一个具有里程碑意义的减碳计划? 如果是,请分享您的计划或实行路径。
未回复B. 您或您的客户是否完成施耐德电气可持续发展学校的所有课程?
未回复2. 您是否有实行数字化?
是
A. 您是否帮助客户部署了集中式公用事业数据管理和监控软件,用于能源和碳分析及报告?
Power Monitoring Expert
B. 在您的帮助下,客户是否会计量主要能源负载,以发现降低能耗和排放的机会?
Yes, Customer is using Energy meters to monitor the Electrical data of major loads, as well as monitoring compressed Air and LNG consumption through flow meters.
C. 您是否进行能源效率的监控?根据设备性能和数据表现,是否有一些见解可以分享?
Customer is keeping an eye on the losses through customized daily report which we have developed specifically for them as per their requirement.
D. 您是否支持客户使用电源管理和监控解决方案来评估电源质量并提高业务弹性和连续性?
Yes, many customers of ours (e.g. Honda Motorcycle & Scooters India Pvt. Ltd., Essar Steel, Essar Power etc.) are using ION and PM meters at their plants to monitor PQ.
E. 您是否代表客户部署了创新解决方案,以最大程度提高其运营效率并实现运营数字化?
Honda is using SMS alarms on Winding and Oil temperatures of all their transformers by using the analog inputs of ION meters.
F. 您是否为客户实施了资产升级和现代化升级,以优化和延长工厂设备的使用寿命并避免排放?
No
G. 您是否为客户实行了电源和流程的数字集成,将其作为最大程度减少能耗并优化流程的一种方法?
Yes. in Honda, apart from Electrical, we have integrated all their utilities like air compressors, air washers, Sewage treatment plant, Waste treatment plant, zero liquid discharge plant, boiler, steam generator etc. and all of them are being monitored and controlled through our software. Daily reports are generated for all these processes and a sharp eye is kept on their efficiency through our system.
3. 您是否采取了减碳措施?
是
A. 您是否正在支持客户使用自动化和能源管理系统来控制其设备和系统?
Yes, in one of the plants in Honda, all the Air Washer exhaust fans and valves, Air compressors are monitored and controlled though our software (Unlimited tag PSO with advance reporting)
B. 在您的帮助下,客户是否实施了提高能效的措施?
Yes, based on the solutions given by us, Honda and Nestle have made impressive savings but as a company policy, the details are not shared with us
C. 您是否支持客户使用可再生能源(PPA、EAC 或现场发电)至少满足其一部分能源需求?
Yes, in one of their plant, Honda has installed roof top solar plant of 2 MW and it is about 15% of their total requirement.
D. 您是否通过场外可再生能源购买协议或能源属性证书来获取能源,以最大程度减少范围 2 排放?
No
E. 在您的帮助下,客户是否正在使用现场可再生能源发电来减少范围 2 排放?
No
F. 您是否为客户实施了储能?
No
G. 您是否为客户提供装备,整合了分散的发电资产,以实现经济价值和电网影响最大化?
No
H. 您是否通过在运营中专注于改善能效来帮助客户减少碳排放?
Yes, we have helped many customers with this, but unfortunately, as a company policy, none of them are allowed to share their data with vendors.
I. 在您的帮助下,客户是否通过专注于改善能效和减碳的现代化项目减少了碳足迹?
yes, but no data is available
J. 您是否帮助客户实施了提高运营能效的措施?
Automatic operation of Air washers and pumps achieved in Honda
K. 您是否与客户的供应商一起帮助客户开展了承诺计划,以减少其范围 3 排放?
No
L. 在您的帮助下,客户是否与上游供应商和下游分销合作伙伴一起采用了承诺计划以跟踪和减少范围 3 排放?
No
M. 您是否支持客户利用数字建模从材料和设备获取了隐含碳相关数据?
No
N. 您是否帮助客户将电动汽车充电基础设施融入到车队、员工和/或客户的运营中?
No
O. 在您的指导下,客户是否将其车队部分车辆改造成电动汽车?
No
P. 您是否支持客户对其部分运营进行电气化改造,以减少范围 1 排放,并支持使用可再生能源来减少碳足迹? 客户运营中的电气化占比是多少?
Yes, done it with Honda but details not available.
Q. 您建议客户购买低隐含碳材料和设备了吗?
No
R. 在您的帮助下,客户是否借助视情况维护来延长设备使用寿命、延迟购买新设备并减少相关的隐含碳排放?
One of our customer has integrated 50 breakers and keeping track of their operation count through PME for timely maintenance of breakers.
S. 根据您的建议,客户是否购买碳补偿以平衡任何范围 1 和范围 3 残余排放?
No
T. 您是否正在通过改善日常运营和关注效率来帮助客户减少用水量?
For Honda we have integrated all their water flow meters (raw water, RO water) with our system and shift wise reports are generated to monitor consumptions. Through this close monitoring, they have been able to improv their operations but and reduce wastages but details are not shared with us.
U. 您是否支持客户根据水可用性风险和预测来监控和调整用水量?
No
V. 您是否帮助客户创建了现场清洁运营优化计划,如以效率为重点的水和废水处理及回收计划?
Yes, Honda is doing it.
W. 在您的帮助下,客户是否采购循环材料,并尽量减少产生运营废物?
No
X. 您是否帮助客户制定了将其基于化石能源的流程向电气化流程转型的计划?
No
Y(i). 您是否帮助客户部署了创新技术或循环业务模式? 请选择所有适用项:
- 帮助客户部署了创新技术以减少其运营的能耗和碳排放?
- 帮助客户部署创新技术以减少用水量?
Y(ii). 这些创新取得了哪些成果?
Please refer to the example of Honda given in previous answers
其他文件(如有)
未回复Translation (when applicable)
未回复
评论