可持续影响力企业奖
如果您是对可持续发展充满热情并承诺践行的施耐德电气客户,我们希望收到您的报名信息。该奖项对于您的团队和企业而言都是一项真正的变革 — 快来提名您的公司吧!
Participate multiple times!
个人
挑战
DTCC
DTCC has been committed to environmental sustainability for many years. We've invested millions of dollars in capital improvements with the intent to reduce our carbon footprint along with operating within a certified environmental management system.
文档
DTCC
公司简介
DTCC has been committed to environmental sustainability for many years. We've invested millions of dollars in capital improvements with the intent to reduce our carbon footprint along with operating within a certified environmental management system.
地点
USA
我是:
大型企业最终用户
细分类型
其他: Financial Services
公司规模
5 亿 - 10 亿欧元
贵公司中是否有人对这些结果的责任人? 如果有,请提供其姓名和电子邮件地址。
Yes, Nicholas Dalesandro. ndalesandro@dtcc.com
我已获得施耐德电气联系人的支持。 如果 "是",请注明您的施耐德电气联系人姓名。
Yes, Andrew Conte
1. 您是否有制定了可持续发展战略?
是
A. 您是否制定了一个具有里程碑意义的减碳计划? 如果是,请分享您的计划或实行路径。
未回复B. 您或您的客户是否完成施耐德电气可持续发展学校的所有课程?
未回复2. 您是否有实行数字化?
是
A. 您是否部署了集中式公用事业数据管理和监控软件,用于能源和碳分析及报告?
DTCC utilizes Schneider's Resource Advisor to monitor all of DTCC's Scope 1, 2 and 3 emissions. Furthermore, DTCC utilizes Schneider Summit Services' Sustainability consulting services to help identify new opportunities for improvement.
B. 您是否通过计量主要能源负载来发现节能和减排的机会?
DTCC utilizes Schneider's PM5000/8000, HDPM6000 meters along with Ecostruxure Buildings monitoring capabilities to track and interpret utilization, which aids in analytical operational/capital project decision.
C. 您是否监控能源效率和设备性能并提供切实可行的见解?
Within Ecostruxure Buildings, our utilization data is categorized by significant energy use (such as lighting, HVAC, etc...). This information is tied to our ISO 50001/14001 management systems in order to identify opportunities for improvement.
D. 您是否使用电源管理和监控解决方案来监控电能质量并提高业务弹性和连续性?
We're actively collecting power quality information, however it's primarily used after the fact for incident root cause analysis. We are not currently modifying operations proactively as a result of power quality inputs.
E. 您是否部署了创新解决方案,以最大程度提高运营效率并实现运营数字化?
We're currently reviewing opportunities to leverage Schneider's Power Expert software for our data centers along with SE/Aveva data analytics to improve our insights into DTCC's energy sources (ie electricity, water, cooling water, gas, etc....)
F. 你们是否实施了资产升级和现代化计划,以优化和延长工厂设备的使用寿命,从而避免排放?
DTCC has recently modernized portions of existing power distribution and UPS equipment. In doing so, we've improved the operational resiliency of our facilities for both concurrent maintainability and incident disruptions. Furthermore, we've leveraged re-use good working order equipment through Schneider's breaker retrofit program to avoid excessive landfill impact.
G. 您是否实行了电力和过程的数字集成解决方案,并将其作为最大程度减少能耗和优化过程的一种方法?
We are piloting a Micro-Grid at one of our facilities which includes on-site PV Solar power generation with the intent to expand to on-site battery storage. With proven success, our intent would be to expand the approach to additional "owned" DTCC properties.
3. 您是否采取了减碳措施?
是
A. 您是否使用自动化和能源管理系统来高效控制设备和系统?
Yes, Schneider Ecostruxure Buildings
B. 您是否实施了提高能源效率的措施?
DTCC has reduced it's enterprise energy consumption by approx 30% since the start of our journey.
C. 您是否使用可再生能源(PPA、EAC 或现场发电)来满足至少一部分能源需求?
We're in the process of constructing an on-site PV Solar generation system.
D. 您是否通过可再生能源购买协议(场外)或能源属性证书来获取能源,以最大程度减少范围 2 排放?
Yes, Schneider Summit Services have aided DTCC in procuring renewable contracts at a portion of our facilities (approx 30%).
E. 您是否使用现场可再生能源发电系统产生的电力,以减少范围 2 排放?
Not yet, in progress.
F. 您是否实施了储能方案以提高弹性,并最大程度减少峰值需求和相关碳排放?
Not yet, in progress.
G. 您是否整合了分散的发电资产,以实现经济价值和电网影响最大化?
Not yet, in progress.
H. 您是否通过改进运营并注重提高能源效率和减碳来实现了碳减排?
未回复I. 您是否通过开展现代化项目,并注重提高能源效率和减碳来实现了碳减排?
未回复J. 您是否实施了提高能源效率的措施?
未回复K. 您是否与供应商一起开展了承诺计划,以减少范围 3 排放?
No but we recognize the opportunity to improve DTCC's monitoring of Scope 3 emissions.
L. 您是否与上游供应商和下游分销商一起开展了承诺计划,以跟踪和减少范围 3 排放?
No, but we're considering SBT alignment in collaboration with Schneider Summit Services.
M. 您是否利用数字建模从材料和设备获取隐含碳相关数据?
No but we recognize the opportunity to improve DTCC's monitoring of embodied carbon.
N. 您是否电动汽车充电基础设施融入到车队、员工和/或客户的运营中?
DTCC has installed EV charging stations at some facilities based on customer demand. We're actively monitoring usage to determine if additional chargers are needed.
O. 您是否将部分车队车辆或现有停车位改造成电动汽车或可供电动汽车使用?
DTCC does not have fleet vehicles.
P. 您是否在一定程度上实现了运营电气化,以减少范围 1 排放并通过使用可再生能源来减少碳足迹?
We're in the process of constructing a PV solar system.
Q. 您是否选择购买隐含碳量低的材料和设备?
R. 您是否借助视情维护来延长设备使用寿命、延迟购买新设备并减少相关的隐含碳排放?
未回复S. 您是否购买了碳补偿,以抵消范围 1 和范围 3 的任何残余排放?
Not at this time. However, we have been acquiring proposals for consideration via Schneider Summit Services team.
T. 您是否通过提高运营效率来减少用水?
DTCC has been actively upgrading all legacy plumbing fixtures to align with present day water consumption standards.
U. 您是否根据水可用性风险预测来监控和调整用水量?
Yes and no. We are actively monitoring to develop but have not yet implemented reduction actions. We intend to be completed with automated data collection via smart water meters enterprise wide in 2024.
V. 您是否拥有以效率为核心的就地清洗、水和废水处理及回收优化计划?
No
W. 您在日常运营中是否会采购循环材料并最大限度减少浪费?
Portions of our IT equipment program participates in circular programs offered (ie Cisco, Dell)
X. 您是否有计划对使用矿物能源的流程实现电气化?
Once the Microgrid is completed, our first line of defense during a power outage will be the battery storage. Once depleted, only then would we move to backup diesel generators if PV is not available.
Y(i). 您是否部署了创新技术或循环商业模式? 请选择所有适用项:
- 部署了创新技术以减少运营的能耗和碳排放
- 部署了创新技术,以用可再生能源取代传统能源
- 部署了创新技术以减少用水
Y(ii). 这些创新取得了哪些成果?
DTCC's enterprise energy consumption has reduced approximately 30% over the past serveral years.
其他文件(如有)
未回复Translation (when applicable)
未回复
评论