可持续影响力企业奖
如果您是对可持续发展充满热情并承诺践行的施耐德电气客户,我们希望收到您的报名信息。该奖项对于您的团队和企业而言都是一项真正的变革 — 快来提名您的公司吧!
Participate multiple times!
个人
挑战
VSB-TU Ostrava, CEET
New technological building represents the demonstration of a functional model of the circular economy, how to use alternative fuels and renewable sources to obtain energy. Part of the project was the design of a microgrid.
文档
VSB-TU Ostrava, CEET
公司简介
New technological building represents the demonstration of a functional model of the circular economy, how to use alternative fuels and renewable sources to obtain energy. Part of the project was the design of a microgrid.
地点
Czech Republic
我是:
大型企业最终用户
细分类型
功率和网格
公司规模
0 - 5,000 万欧元
贵公司中是否有人对这些结果的责任人? 如果有,请提供其姓名和电子邮件地址。
Stanislav Mišák, stanislav.misak@vsb.cz
我已获得施耐德电气联系人的支持。 如果 "是",请注明您的施耐德电气联系人姓名。
Eduard Křiklava
1. 您是否有制定了可持续发展战略?
否
A. 您是否制定了一个具有里程碑意义的减碳计划? 如果是,请分享您的计划或实行路径。
未回复B. 您或您的客户是否完成施耐德电气可持续发展学校的所有课程?
未回复2. 您是否有实行数字化?
是
A. 您是否部署了集中式公用事业数据管理和监控软件,用于能源和碳分析及报告?
ProCop, Ecostructure Microgird Operator and Adviser
B. 您是否通过计量主要能源负载来发现节能和减排的机会?
The electricity and heat consumption of individual buildings is measured and regularly evaluated, and subsequently electricity savings and other measures are proposed.
C. 您是否监控能源效率和设备性能并提供切实可行的见解?
Energy efficiency is monitored for individual buildings and measures are continuously proposed to reduce energy consumption.
D. 您是否使用电源管理和监控解决方案来监控电能质量并提高业务弹性和连续性?
We monitor the quality of electricity and reliability of supply at selected locations of the local distribution system and are regularly evaluated. Corrective action is taken when necessary.
E. 您是否部署了创新解决方案,以最大程度提高运营效率并实现运营数字化?
We operate a digital system for processing all data, most technologies are fully digitized.
F. 你们是否实施了资产升级和现代化计划,以优化和延长工厂设备的使用寿命,从而避免排放?
All technologies are regularly upgraded to be at the global cutting edge in research.
G. 您是否实行了电力和过程的数字集成解决方案,并将其作为最大程度减少能耗和优化过程的一种方法?
We have implemented complete energy management, which monitors electricity consumption, including complete reporting.
3. 您是否采取了减碳措施?
是
A. 您是否使用自动化和能源管理系统来高效控制设备和系统?
未回复B. 您是否实施了提高能源效率的措施?
未回复C. 您是否使用可再生能源(PPA、EAC 或现场发电)来满足至少一部分能源需求?
We have onsite generation (PV system, Wind Power Plants, Fuel Cell, Stirling Engine, CHP). About 50% of electricity is covered from own renewable energy sources.
D. 您是否通过可再生能源购买协议(场外)或能源属性证书来获取能源,以最大程度减少范围 2 排放?
未回复E. 您是否使用现场可再生能源发电系统产生的电力,以减少范围 2 排放?
About 50% of electricity is covered from own renewable energy sources.
F. 您是否实施了储能方案以提高弹性,并最大程度减少峰值需求和相关碳排放?
We have several battery storage systems installed,
G. 您是否整合了分散的发电资产,以实现经济价值和电网影响最大化?
未回复H. 您是否通过改进运营并注重提高能源效率和减碳来实现了碳减排?
未回复I. 您是否通过开展现代化项目,并注重提高能源效率和减碳来实现了碳减排?
未回复J. 您是否实施了提高能源效率的措施?
未回复K. 您是否与供应商一起开展了承诺计划,以减少范围 3 排放?
未回复L. 您是否与上游供应商和下游分销商一起开展了承诺计划,以跟踪和减少范围 3 排放?
未回复M. 您是否利用数字建模从材料和设备获取隐含碳相关数据?
New buildings are designed using BIM, we have facility management in place.
N. 您是否电动汽车充电基础设施融入到车队、员工和/或客户的运营中?
We have installed charging stations for electric cars for the company fleet, including one filling station for hydrogen-powered vehicles.
O. 您是否将部分车队车辆或现有停车位改造成电动汽车或可供电动汽车使用?
We have a fleet of electric powered vehicles, about 10% of the vehicles. The parking infrastructure for these vehicles is gradually being implemented.
P. 您是否在一定程度上实现了运营电气化,以减少范围 1 排放并通过使用可再生能源来减少碳足迹?
未回复Q. 您是否选择购买隐含碳量低的材料和设备?
未回复R. 您是否借助视情维护来延长设备使用寿命、延迟购买新设备并减少相关的隐含碳排放?
未回复S. 您是否购买了碳补偿,以抵消范围 1 和范围 3 的任何残余排放?
未回复T. 您是否通过提高运营效率来减少用水?
未回复U. 您是否根据水可用性风险预测来监控和调整用水量?
未回复V. 您是否拥有以效率为核心的就地清洗、水和废水处理及回收优化计划?
未回复W. 您在日常运营中是否会采购循环材料并最大限度减少浪费?
未回复X. 您是否有计划对使用矿物能源的流程实现电气化?
未回复Y(i). 您是否部署了创新技术或循环商业模式? 请选择所有适用项:
- 部署了创新技术以减少运营的能耗和碳排放
- 部署了创新技术,以用可再生能源取代传统能源
- 部署了创新技术以减少用水
- 部署了创新技术或循环商业模式
Y(ii). 这些创新取得了哪些成果?
未回复其他文件(如有)
未回复Translation (when applicable)
未回复
评论